What's New!

In this section, we will regularly feature the newest and latest product innovation, installation success stories, corporate milestones. If you would like to receive our monthly email blast, please sign up here.

INTRODUCING EPIC® ULTRA CONNECTOR HOUSING FOR HARSH ENVIRONMENTS

epic ultra

Lapp recently introduced the next generation industrial connector housing, EPIC® ULTRA. This new housing was engineered to meet the needs of harsh industrial applications. Its unique design and  construction makes it

 

Ideal for Use in Extreme Environments

 

  • Scratch, impact, and corrosion resistant
  • Dust & water tight to IP65
  • Immunity from electrical interference

 

APPLICATION RANGE:

 

  • In EMC and EP washdown critical environments
  • For stationary and motion aplpications in machine building and material handling
  • Other industry applications include machine tool, bottling and printing machines, carwash, food processing, etc...

LAPP INTRODUCES ITS LATEST MOTOR & DRIVE CABLE

Homepage VFD

ÖLFLEX® VFD XL is an extremely oil resistant and robust, shielded motor cable for VFD drives. The jacket is also excellent at low temperatures, passing both the UL -25ºC Cold Impact and the -40ºC Cold Bend tests. Stranding complies with both North American and European requirements. The stranding provides larger CMA, resulting in lower DC resistance compared to standard AWG sizes. The enhanced electrical characteristics of XLPE insulation provide problem free performance where precision control is critical.

 

Recommended Applications:
VFD drive and motor connections, web presses, HVAC, conveyors, longer length installations, and any on/off applications using a VFD drive and motor.

 

Application Advantage:
• Class 5 Global Stranding
• XLPE insulation for better precision control
• Industrial grade PVC jacket, passing Oil Res I & II
• Outer jacket will withstand UL -25ºC Cold Impact & UL -40ºC Cold Bend tests
• Designed for environmentally harsh conditions
• UL TC-ER & c(UL)CIC/TC

THE LAPP GROUP CELEBRATES 50th ANNIVERSARY OF ÖLFLEX

50 Years OLFLEX Ice Scultpture

The Lapp Group commemorated the 50th anniversary of their signature brand ÖLFLEX®.

 

ÖLFLEX was the world’s first industrially manufactured power and control cable, and the first ever cable with color-coded conductors. Ever since it was invented in 1959, ÖLFLEX has been synonymous with quality, reliability and speed. To celebrate this, the Lapp Group is holding the ÖLFLEX World Tour, which means that an ÖLFLEX cable drum is visiting various Lapp sites around the globe. On April 13 2011, the ÖLFLEX World Tour made its American stop at the Lapp Group’s American headquarters in Florham Park, New Jersey.

MORE VALUE, MORE BENEFITS, MORE THAN YOU IMAGINE

unternehmen geschichte 03 OELFLEX swP 02

Just when you thought our cables couldn't get any better, they have.

 

Now, with Lapp innovative ÖLFLEX® Tray II with enhanced oil and temperature resistance, our Tray Cables offer an even greater level of performance and longevity resulting in higher value and cost savings.

 

 

DEADLINES JUST MET THEIR MAKER WITH LAPP QUICK SHIP PROGRAM

HBE10HPTopEHoodDB

When you need it yesterday. Our most popular connectors and strain relief cable glands in 48 hours or less.

 

The new Lapp Group North America "Quick-Ship" Program provides off-the-shelf delivery of our most popular connectors and strain relief cable glands typically in 48 hours or less.

Our inventory resources are available to help solve your immediate needs and minimize costly downtime.

Most of these products are direct replacements for those offered by other manufacturers. So when you need it in a rush, look to Lapp Group North America for the solution.

 

Call our Inside Sales department at 800-774-3539 for help in selecting a product. For a list of participating components, click here.

 

 

SKINTOP® CUBE: SIMPLE. FLEXIBLE. SAFE.

SKINTOP Cube

With SKINTOP® CUBE, it doesn't get any quicker or easier than this!

 

There are number of multi-cable bushing systems on the market, however, Lapp Group has now succeeded in making the basic principles of a multi-cable bushing system even easier, faster and safer.

The patented SKINTOP® CUBE flexible clip modules provide extremely quick and easy installation with far better sealing and clamping capabilities. Additionally, service to the cables is greatly simplified, as removing the frame from the enclosure is not necessary when updating cables.

 

Call our Inside Sales department at 800-774-3539 for help in selecting the right module or click here to download the complete brochure.